Conduit Bending Instructions (EMT Bender)


Accurate Stubs

Conduit Bending: Accurate Stubs

Subract take-up from desired stub height. This gives distance at which to place B on bender from the end of the tube. To make 11", 90° bend with 1/2" tube, allow for 5" for take-up as shown on diagram.
With 3/4" tube, allow 6"
With 1" tube, allow 8"

True Offsets

Conduit Bending: True Offsets

Line up arrow on either side of hook with guideline and make 45° bend in tube. Reverse tube in bender and adjust so that X is lined up with inch-mark on bender corresponding to depth of offset desired. Line up guide-line with opposite arrow and make second 45° bend. A true offset, in the sname plane, will result between X and Y.

Back-to-Back Bends

Conduit Bending: Back to back Bends

Make stub bend at X with guide-line centered on either arrow located on side of hook. Measure distances from X to Y on tube.

Reverse bender and put A on bender at Y on tube. Line up guide-line with opposite arrow than used when making first stub and make second bend.

Saddle Bends

Conduit bending: Saddle Bends

C -- Center of finished Saddle Bend
X -- Double of the diameter of round object from C
Y -- Double of the diameter of round object from C

Saddle Bend, Step 1

Saddle Bend step one: make a 45 degree bend

Place tube in bender so that "C" on tube is at notch on bender and make a 45 bend. (A 45 bend is reached when bender handle is at a right angle to the tube.)

Saddle Bend, Step 2

Saddle Bend step two: return bend, 22.5 degrees

Reverse tube in bender and place B on bender at X on tube. Make return bend of 22 1/2 . Duplicate procedure placing B on bender at Y on tube and complete saddle by making another 22 1/2 bend.

Finished bend neatly saddles round object

A completed Saddle Bend

Proper alignment of the guide-line with arrows on bender hook will result in the saddle being in a straight line.

To Straighten

How to straighten conduits

Place handle of bender over stub or piece of pipe that will fit inside and push down to the floor in one full sweep.