The Electric Times - Current Sales Events at Elliott Electric Supply



 
Electric Times banner header
Electric Times banner


April 2025 Electric Times


Elliott Electric Supply has over 180 location in 13 states! Visit ElliottElectric.com to find a store near you!
We hope to see you soon!


Elliott Electric Supply logo


We Deliver... Lower Cost, Quality Products, & Personal Service


:::


April 2025 Eaton Res Ad


Eaton's CH Main Lug Loadcenters are designed with the installer in mind!


They feature a plug -on neutral design that provides time and labor savings by eliminating the pigtail. Backed out neutral screws, increased gutter space and self -leveling offset tabs are just a few of the features that prioritize a cleaner and simpler install. Contact your local Elliott Electric Supply for more information about Eaton's CH main Lug Loadcenters!


Eaton logo


:::


April 2025 Eaton Com Ad


April showers? No problem! Check out Eaton's weatherproof and while-in-use boxes and covers!


Eaton's weatherproof covers are designed for longevity in virtually any outdoor, indoor, wet or damp location. Patented corner ball joints allow for vertical or horizontal mounting with zero disassembly and rugged UV-resistant polycarbonate covers and backs protect without cracking or corrosion. Hurry to your local Elliott Electric Supply to check out Eaton's Weatherproof Boxes and Covers!


Eaton Logo


:::


Southwire VOM Ad


The vendor of the month for our Eastern and Western Region is Southwire!


At participating Elliott Electric Supply stores, you could win a medium Big Green Egg with the purchase of a Southwire Extension Cord. Southwire Extension Cords come in either 50ft or 100ft and are built to stay flexible under the most extreme conditions. They are designed to withstand moisture, abrasion, chemicals and oils for survival in the toughest of environments. They feature a clear molded plug with a power indicator light in the female receptacle to show that the power is on and ready to use!


Southwire Logo


:::


ABB VOM Ad


The vendor of the month for our central region at Elliott Electric Supply is ABB!


ABB is featuring three products this month. Carlon Blue Fan-rated Ceiling Boxes helps keep homes safer. Carlon Electrical non-Metallic tubing fittings help make your job easier. T&B Liquidtight non-metallic lock nuts complete a non-metallic solution to help prevent corrosion. Visit your local Elliott Electric Supply today to check out these ABB Products!


ABB logo


:::


Klein Tools Ad


Klein Tools Modbox Utility Cart has a Modbox rail to hold Modbox accessories!


It also has a 39 inch overall height which makes it taller than most carts and more comfortable when using the top shelf as a work surface. It has 6 inch rubber caster wheels to effortlessly move almost anything anywhere and a cart handle that includes two cup holders and multiple compartments. With a 500 pound capacity, don't miss out on the Klein Tools Modbox Utility Cart at your local Elliott Electric Supply.


Klein Tools logo


:::


ASD Ad


Experience ASD's lighting evolution with their LED Flushmount!


Available in multiple designs, the LED Flushmount Lights have 3 color or 5 color temperature options, seamless triac dimming to adjust brightness level and save energy, acrylic lens with even light distribution and 2.75" and 3.5" mounting holes for advanced installation options. Check out ASD's LED Flushmount Lights at your local Elliott Electric Supply today!


ASD Logo


:::


Dottie Ad


Dottie's Multi-purpose Tuff Towel features a powerful yet gentle cleaning formula that can remove paint, ink, tar, adhesives, sealant, grease and oil from tools, equipment, and hands!


The dual-purpose texture removes stubborn adhesives and grime by utilizing the green abrasive spun lace fibers on one side. The opposing side of the towel is made from soft yet durable polyester, which gently cleans your hands. The unique formula contains a fresh citrus scent and aloe that leaves the skin moisturized. Dottie's Multipurpose Tuff Towels allow you to keep clean on the jobsite without the need for water. Visit your local Elliott Electric Supply to check out Dottie's Multi-purpose Tuff Towels!


Dottie Logo


:::


Cooper Lighting Ad


Cooper Lighting's Metalux APVT LED series is an energy-efficient industrial luminaire that combines the rugged construction of a vaportite with selectable CCT and lumen output!


It is ideal for interior and exterior applications, including parking garages, canopies, warehouses and light commercial spaces. Explore the APVT LED series at Elliott Electric Supply today!


Cooper Lighting Logo


:::


Kraloy Ad


Kraloy, the most robust ENT system in the industry!


Check out your local Elliott Electric Supply for Kraloy products!


Kraloy Logo


:::


April Promotion ad


Save the date for Elliott Electric Supply's 30th Customer Appreciation Big Bass Classic!


This year's Big Bass Classic will be held at Lake Fork's, Lake Fork Marina on the weekend of April 12th and 13th. During Saturday's vendor trade show, visit with other tournament anglers, browse through products from our suppliers and enjoy good food and a cold drink on us while checking in for Sunday's tournament. It's all part of the fun at the 30th Big Bass Classic weekend at Lake Fork's Lake Fork Marina. Don’t miss it!


EES logo


:::

Picjup Online Orders ad


In a hurry?


Order your items online at elliottelectric.com or our Customer Mobile app and pick them up at one of our convenient locations!


EES logo


:::


Follow us on

Facebook logo Twitter logo Instagram logo

PO Box 630610 Nacogdoches, TX 75963
Click here to unsubscribe.


:::