Delivery Driver Opening


← Back to Job Listings

An Elliott Electric Supply Store

Delivery Driver in Conway, AR

Job Description:

Transport materials along assigned routes, operating vehicles safely and professionally. Provide excellent customer service through prompt, courteous deliveries. Secure loads for safe transit and unload materials at each stop, verifying accuracy and condition. Perform daily vehicle inspections to ensure maintenance and safety. Will also handle general warehouse duties as assigned. 

This is a safety-sensitive position requiring constant awareness. Employment is contingent on a pre-employment drug test screening for amphetamines, cocaine, marijuana (THC), methamphetamines, opiates, oxycodone, and phencyclidines per HHS/SAMHSA cutoff levels. Note: under USDOT rule 49 CFR Part 40.151(e), medical marijuana is not an acceptable explanation for a THC-positive result.

Why join us? Competitive pay; Medical, dental & vision insurance; 401(k) plan; Vacation, 4 personal days, and 6 paid holidays; Employer-paid life insurance; optional voluntary family life coverage; Short- & long-term disability; Optional accident, critical illness, and hospital indemnity plans

Qualifications:

High school diploma or equivalent is preferred. Must demonstrate proficiency with Android or iOS operating systems. Valid driver’s license from the state of residence is required, minimum of three (3) years of driving history. A satisfactory motor vehicle record (MVR), with no Type A violation within the past seven years; a speeding violation of 15+ mph over the limit within the past three years; or more than one (1) Type B violations within the past three years.  A minimum of one (1) year of experience operating a commercial motor vehicle with a gross vehicle weight rating (GVWR) of 10,001 lbs. or greater within the last 36 months. Strong skills in reading, writing, performing basic calculations, data entry, reasoning, and analysis are essential. The ability to work independently while managing a variety of tasks accurately and with attention to detail in a team-oriented environment is required.

Physical Requirements: Must meet the physical qualifications to operate a motor vehicle in accordance with Section 391.41 of the Federal Motor Carriers Safety Administration (FMCSA). Regular visits to customer sites will expose the employee to various weather conditions and environmental factors. Awareness of and adherence to each customer’s safety protocols is essential, as there may be occasional exposure to hazards such as loud noise or moving machinery. The role requires frequent walking, bending, squatting, climbing, and kneeling. Occasional pushing, pulling, and reaching are necessary. Handling and lifting of objects up to 50 pounds is expected, with occasional lifting of up to 75 pounds.



Job Type: Full-Time Contact: Caleb Crittenden (501)336-8444

Location: Conway, AR (99)

Apply For This Position