Control Transformer Selection Guide
Selection Procedure
The following steps will ensure that the secondary voltage
delivered by your transformer will be either 85%, 90% or 95% of the nameplate secondary voltage under maximum inrush conditions,
at the rated input voltage.
Step 1:
Calculate the total sealed (steady state) VA load of your control circuit. This is done by adding
the continuous VA requirements of the maximum number of components that will be energized at any given time, including non-inductive
as well as inductive components. For sealed VA data,
see the Component VA Chart below.
Step 2:
Calculate the peak inrush VA for your control circuit.
- Analyze the sequence of operation of all components.
- Add together the
inrush VA ratings of the components
that will be energized simultaneously.
- Determine the peak - or maximum simultaneous - inrush VA load that the transformer will "see."
The VA requirements for indicating lights, timers, and other non-inductive components which do not have an inrush VA also should be included since
they will present a load to the transformer at the time of maximum inrush.
Step 3:
Calculate the transformer selection inrush VA. Use the following formula:
Selection Inrush VA = √((VA Sealed)2 + (VA Inrush)2)
NOTE: Transformer selection inrush VA also can be determined by adding the inrush VA and sealed VA arithmetically,
but this usually results in an oversized transformer.
Step 4:
Determine the correct transformer nameplate VA Rating.
Refer to the Inrush/Regulation Data Chart
:
- If the line supply to the transformer is fairly stable (does not vary more than 5%), use the 90% secondary voltage column -
the 90% column is most commonly used.
- If the line supply voltage varies up to 10%, use the 95% voltage regulation column.
To determine the correct VA transformer rating, go down the column until you arrive at the inrush VA rating closest to, but not
less than, the transformer selection inrush VA calculated in Step 3. The left-hand column of the table will give the corresponding
transformer nameplate VA rating.
NOTE: When evaluating supply-line stability remember that supply-line voltage drop frequently is associated with motor-starting
inrush current. When motors and motor controls are connected to a common feeder, the controls will experience a momentary
voltage dip when the motor starts. This reduces the control transformer voltage supplied to the motor starting contactor and
may cause the contractor to chatter or drop out.
Component VA Chart for Starters, Contactors, Relays, and Timers
Device |
Inrush |
Sealed |
VAR |
Watts |
VA |
VAR |
Watts |
VA |
FREEDOM SERIES STARTERS AND CONTACTORS:
AE16, AN16, AE56, CE15, CN35, CE55, CN55, MCE15 |
IEC Sizes A‑C |
64 |
49 |
80 |
7.1 |
2.4 |
7.5 |
IEC Sizes D‑F |
78 |
65 |
100 |
9.2 |
3.1 |
10.0 |
IEC Sizes G‑K |
210 |
95 |
230 |
27.0 |
7.8 |
28.0 |
IEC Sizes L‑N |
374 |
112 |
390 |
48.0 |
13.0 |
49.8 |
IEC Sizes P‑S |
1132 |
240 |
1158 |
96.0 |
27.2 |
100.0 |
NEMA Size 00 |
64 |
49 |
80 |
7.1 |
2.4 |
7.5 |
NEMA Size 0 |
78 |
65 |
100 |
9.2 |
3.1 |
10.0 |
NEMA Sizes 1‑2 |
210 |
95 |
230 |
27.0 |
7.8 |
28.0 |
NEMA Size 3 |
374 |
112 |
390 |
48.0 |
13.0 |
49.8 |
NEMA Sizes 4‑5 |
1132 |
240 |
1158 |
96.0 |
27.2 |
100.0 |
NEMA Size 6 |
868 |
1345 |
1600 |
11.0 |
21.0 |
25.0 |
CITATION CONTACTORS AND STARTERS:
A10, A50, B10, B50, C10, C50 |
Size 00: Series C1 |
64 |
49 |
80 |
7.1 |
2.4 |
7.5 |
Sizes 0‑1 |
81.5 |
63 |
103 |
18.7 |
7.0 |
20.0 |
Size 2 |
115 |
80 |
140 |
22.0 |
9.3 |
24.0 |
Size 3 |
374 |
112 |
390 |
48.0 |
13.0 |
49.8 |
Sizes 4‑5 |
1132 |
240 |
1158 |
96.0 |
27.2 |
100.0 |
Size 6: Series C1 |
868 |
1345 |
1600 |
11.0 |
21.0 |
25.0 |
Size 7: Series B1 Interposing Relay |
29 |
68 |
74 |
5.1 |
6.8 |
8.5 |
Size 7: Series B1 Main Contactor |
6275 |
2989 |
6950 |
170.0 |
60.0 |
180.0 |
Size 8: Series B1 Main Coil |
1262 |
2100 |
2450 |
56.0 |
50.0 |
75.0 |
RELAYS |
Type AA (1‑2 Pole) |
18.0 |
8.5 |
20.0 |
8.0 |
6.6 |
11.0 |
Type D15 |
64.0 |
49.0 |
80.0 |
7.1 |
2.4 |
7.5 |
Type M (2‑12 Pole) |
122.0 |
95.0 |
155.0 |
20.0 |
9.0 |
22.0 |
Type M Latch Coil |
36.5 |
18.5 |
41.0 |
13.0 |
11.0 |
17.0 |
Type MRD |
-- |
168.0 |
-- |
-- |
13.2 |
13.2 |
Type MRD Ltc. Coil |
-- |
21.6 |
-- |
-- |
21.6 |
-- |
Type R |
-- |
6.0 |
6.0 |
-- |
6.0 |
6.0 |
Type RM‑Set |
-- |
-- |
-- |
-- |
3.5 |
3.5 |
Type RM‑Release |
-- |
-- |
-- |
-- |
3.1 |
3.1 |
Type TF |
3.0 |
3.0 |
4.0 |
3.0 |
3.0 |
4.0 |
Type TH |
4.0 |
4.0 |
5.0 |
4.0 |
4.0 |
5.0 |
TIMERS |
Type D80 |
60.0 |
67.0 |
90.0 |
18.0 |
6.0 |
19.0 |
Type D80 with Installed Contacts |
89.0 |
95.0 |
130.0 |
20.0 |
7.0 |
21.0 |
Sealed Devices
Device |
Sealed |
VAR |
Watts |
VA |
FREEDOM SERIES STARTERS AND CONTACTORS:
AE16, AN16, AE56, CE15, CN35, CE55, CN55, MCE15 |
IEC Sizes A‑C |
7.1 |
2.4 |
7.5 |
IEC Sizes D‑F |
9.2 |
3.1 |
10.0 |
IEC Sizes G‑K |
27.0 |
7.8 |
28.0 |
IEC Sizes L‑N |
48.0 |
13.0 |
49.8 |
IEC Sizes P‑S |
96.0 |
27.2 |
100.0 |
NEMA Size 00 |
7.1 |
2.4 |
7.5 |
NEMA Size 0 |
9.2 |
3.1 |
10.0 |
NEMA Sizes 1‑2 |
27.0 |
7.8 |
28.0 |
NEMA Size 3 |
48.0 |
13.0 |
49.8 |
NEMA Sizes 4‑5 |
96.0 |
27.2 |
100.0 |
NEMA Size 6 |
11.0 |
21.0 |
25.0 |
CITATION CONTACTORS AND STARTERS:
A10, A50, B10, B50, C10, C50 |
Size 00: Series C1 |
7.1 |
2.4 |
7.5 |
Sizes 0‑1 |
18.7 |
7.0 |
20.0 |
Size 2 |
22.0 |
9.3 |
24.0 |
Size 3 |
48.0 |
13.0 |
49.8 |
Sizes 4‑5 |
96.0 |
27.2 |
100.0 |
Size 6: Series C1 |
11.0 |
21.0 |
25.0 |
Size 7: Series B1 Interposing Relay |
5.1 |
6.8 |
8.5 |
Size 7: Series B1 Main Contactor |
170.0 |
60.0 |
180.0 |
Size 8: Series B1 Main Coil |
56.0 |
50.0 |
75.0 |
RELAYS |
Type AA (1‑2 Pole) |
8.0 |
6.6 |
11.0 |
Type D15 |
7.1 |
2.4 |
7.5 |
Type M (2‑12 Pole) |
20.0 |
9.0 |
22.0 |
Type M Latch Coil |
13.0 |
11.0 |
17.0 |
Type MRD |
-- |
13.2 |
13.2 |
Type MRD Ltc. Coil |
-- |
21.6 |
-- |
Type R |
-- |
6.0 |
6.0 |
Type RM‑Set |
-- |
3.5 |
3.5 |
Type RM‑Release |
-- |
3.1 |
3.1 |
Type TF |
3.0 |
3.0 |
4.0 |
Type TH |
4.0 |
4.0 |
5.0 |
TIMERS |
Type D80 |
18.0 |
6.0 |
19.0 |
Type D80 with Installed Contacts |
20.0 |
7.0 |
21.0 |
Inrush Devices
Device |
Inrush |
VAR |
Watts |
VA |
FREEDOM SERIES STARTERS AND CONTACTORS:
AE16, AN16, AE56, CE15, CN35, CE55, CN55, MCE15 |
IEC Sizes A‑C |
64 |
49 |
80 |
IEC Sizes D‑F |
78 |
65 |
100 |
IEC Sizes G‑K |
210 |
95 |
230 |
IEC Sizes L‑N |
374 |
112 |
390 |
IEC Sizes P‑S |
1132 |
240 |
1158 |
NEMA Size 00 |
64 |
49 |
80 |
NEMA Size 0 |
78 |
65 |
100 |
NEMA Sizes 1‑2 |
210 |
95 |
230 |
NEMA Size 3 |
374 |
112 |
390 |
NEMA Sizes 4‑5 |
1132 |
240 |
1158 |
NEMA Size 6 |
868 |
1345 |
1600 |
CITATION CONTACTORS AND STARTERS:
A10, A50, B10, B50, C10, C50 |
Size 00: Series C1 |
64 |
49 |
80 |
Sizes 0‑1 |
81.5 |
63 |
103 |
Size 2 |
115 |
80 |
140 |
Size 3 |
374 |
112 |
390 |
Sizes 4‑5 |
1132 |
240 |
1158 |
Size 6: Series C1 |
868 |
1345 |
1600 |
Size 7: Series B1 Interposing Relay |
29 |
68 |
74 |
Size 7: Series B1 Main Contactor |
6275 |
2989 |
6950 |
Size 8: Series B1 Main Coil |
1262 |
2100 |
2450 |
RELAYS |
Type AA (1‑2 Pole) |
18.0 |
8.5 |
20.0 |
Type D15 |
64.0 |
49.0 |
80.0 |
Type M (2‑12 Pole) |
122.0 |
95.0 |
155.0 |
Type M Latch Coil |
36.5 |
18.5 |
41.0 |
Type MRD |
-- |
168.0 |
-- |
Type MRD Ltc. Coil |
-- |
21.6 |
-- |
Type R |
-- |
6.0 |
6.0 |
Type RM‑Set |
-- |
-- |
-- |
Type RM‑Release |
-- |
-- |
-- |
Type TF |
3.0 |
3.0 |
4.0 |
Type TH |
4.0 |
4.0 |
5.0 |
TIMERS |
Type D80 |
60.0 |
67.0 |
90.0 |
Type D80 with Installed Contacts |
89.0 |
95.0 |
130.0 |
Inrush/Regulation Data
Transformer VA Rating at 55℃ |
Inrush VA‑40% Power Factor |
At 95% Secondary Voltage |
At 90% Secondary Voltage |
At 85% Secondary Voltage |
60 |
137 |
185 |
227 |
95 |
242 |
329 |
409 |
105 |
294 |
407 |
512 |
180 |
592 |
842 |
1071 |
225 |
929 |
1312 |
1663 |
275 |
1271 |
1801 |
2288 |
320 |
1581 |
2224 |
2816 |
380 |
2124 |
3048 |
3895 |
550 |
3196 |
4604 |
5896 |
850 |
5500 |
7914 |
10141 |
1100 |
8382 |
12067 |
15477 |
1500 |
11100 |
16066 |
21032 |
2000 |
21820 |
24356 |
41100 |
3000 |
29123 |
32770 |
59997 |
5000 |
74595 |
111000 |
145000 |
7500 |
104000 |
162000 |
219000 |
10000 |
111000 |
166000 |
237000 |
Inrush/Regulation Data: 95% and 90% Secondary Voltage
Transformer VA Rating at 55℃ |
Inrush VA‑40% Power Factor |
At 95% Secondary Voltage |
At 90% Secondary Voltage |
60 |
137 |
185 |
95 |
242 |
329 |
105 |
294 |
407 |
180 |
592 |
842 |
225 |
929 |
1312 |
275 |
1271 |
1801 |
320 |
1581 |
2224 |
380 |
2124 |
3048 |
550 |
3196 |
4604 |
850 |
5500 |
7914 |
1100 |
8382 |
12067 |
1500 |
11100 |
16066 |
2000 |
21820 |
24356 |
3000 |
29123 |
32770 |
5000 |
74595 |
111000 |
7500 |
104000 |
162000 |
10000 |
111000 |
166000 |
Inrush/Regulations Data: 85% Secondary Voltage
Transformer VA Rating at 55℃ |
Inrush VA‑40% Power Factor |
At 85% Secondary Voltage |
60 |
227 |
95 |
409 |
105 |
512 |
180 |
1071 |
225 |
1663 |
275 |
2288 |
320 |
2816 |
380 |
3895 |
550 |
5896 |
850 |
10141 |
1100 |
15477 |
1500 |
21032 |
2000 |
41100 |
3000 |
59997 |
5000 |
145000 |
7500 |
219000 |
10000 |
237000 |
Warning: When using this information to perform electrical work, call a licensed electrician and consult the NEC® for safety.
All licensed electricians have passed examinations covering the National Electric Code®, know state and local building codes, and may carry insurance to cover damages.